Input field and validation
Hello!
Sometimes we noticed non-validate value with input field item.
Indeed, operators have to use "enter button" to validate their values otherwise the older values stay...
Do you have an idea to add a validation button or anything else to be sure the new entered value is validate by operators.
Hope it is clear for you.
Thanks in advance
Regards
Answers
Already option exists. Im not sure which version of 800xA you are using?
Im not sure when this feature was introduced but atleast AFAIK from 5.1 FP4,Whenever we configure Input field by choosing its Datatype Property, (Real,Time,etc.,) the input field takes only those characters. If you enter some other character, it highlights with a red box (even before Operator Clicks enter button) showing the operator that the entered characters are invalid. If the operator ignores the red box and presses enter button, old value will be retained.
Thanks
Add new comment