How to Simulate Panel Builder With SoftController
Can i simulate software for Panel Builder 800, Version 5.1/0 (Build 353) Together with Compact Control Builder AC800M, Version 5.1/1 (Build 5.1.100.13) that use SoftController ?
Thank you.
Voted best answer
Hello
it is possible to use Softcontroller with Compact control builder for AC800M.
But i am not sure about the panel builder interface with simulated one
Answers
Check following issue in this forum:
How to configure Soft Controller in Compact control builder AC 800M(Ver 5.1) for testing program.
1. Configure Control Builder and Soft controller.
2. Download the program to the specified soft controller.
3. Create a project in Panel Builder and add the controller to the project.
4. Connect the tags through OPC browser.
5. Build the project in Panel builder and Run.
2. Download the program to the specified soft controller.
3. Create a project in Panel Builder and add the controller to the project.
4. Connect the tags through OPC browser.
5. Build the project in Panel builder and Run.
by AMEC004 Rank: 3685 on 5/26/2015 12:34:25 AM | Like (0) | Report
Thank you for good suggestion, But I would like to simulate program together between Panel Builder 800 and Compact Control Builder AC800M, How can i do ?
Please suggest me.
Thank you.
by Govindaraj
Simulation function in Panel Builder 800 software is only used to test graphic displays and navigation. If you need real time values from controller you need to use physical hardware.
by AMEC004 Rank: 3685 on 5/26/2015 2:13:46 AM | Like (0) | Report
Thank you.
Add new comment