control commands form SCADA on 61850
I am having REF relay. From scada i want to give control command to relay. This is other
than goose. And if this command is reveived and any one binary input is high, with such a condition i want to operate binary output. Is such control possible in REF? If yes then through which logical node i have to use?
Answers
Hi,
try to check next documents, you can find answers inside:
BTW - there can be suitable to join any course. IEC61850 Configuration (on substation level) is quite complex area...
Hope this help.
by admin Rank: 37 on 5/25/2015 1:53:28 AM | Like (0) | Report
You are using system 800xA? or some ABB or other scada system ?
Add new comment