Control Network redundancy on PP845 when using with AC 800M controlelrs
We are going to use PP845 in our project, In the manuals for PP845, it is mentioned that these displays can be completely integrated with AC 800M controllers over control network. My question is, we have redundant control network CN1 and CN2" in a AC800M controller. Can the PP845 have redundant ports so that we have redundancy with network point of view. i.e. even if i lose network on CN1, my communication still runs on the CN2 port. Any view on this is deeply appreciated..
Answers
PP845 not supports redundant networks. It only can be connected to the CN1 in your case.
You can Refer Answers posted for "How can I use Process Panels (PP845) with redundant AC 800M controllers?"
Add new comment