Is the any way to use codesys 3.5 with ac500 ?
hi, i really want to program using object oriented programming but this cant be achived in codesys 2 is there any way to use codesys 3.5 with AC500 ?
Voted best answer
Hi! There're so called v3 AC500 PLCs which are programmed in CoDeSys 3.5 (both hardware configuration and logic). Designation of those CPUs are 4 digits: PM5630, PM5650, PM5670, PM5675.
Answers
Hi
IMHO no, actually ABB use Codesys 3.0 in the Automation Builder version 2.0x but only for the new cpu like PM 56XX
Probably in the next future?
Have a nice day
Add new comment