AC110 online connection
Dears,
i have AC110 controller with OPT1 and HPC 502 liberary for AVR generator control, my ES130 station is damaged, i have a backup from supplier for the application logic (AAX, BAX, Cxx), i installed APB, FCB on another engineering station, when trying to connect to node it gives me program mismatch. i want a method to compare online logic running on CPU with my backup as i'm not sure that both logics are the same
Answers
You can't.
There is no way to download the program from the controller. You can only compile the Source code and load that to the controller. If you do not have your own backups then you have to hope and trust that the .AAX and BAX files you got from your supplier are up to date.
Have you tried asking a specialist data recovery company what they can get from the ES130 hard drive ? Unless the drive is lost or otherwise physically damaged its usually possible to recover all or most of the data.
Next time - take backups !
Add new comment