Application hangs when workstation connected to abb 800xa server
While connected to the server and starts the application for operator workstation grahics page then the application hangs but the workstation still OK. Other clients also not effected.
Answers
Hi,
This could be due to a networking issue. In one project we tried to bridge two network ethernet ports for redundancy in all nodes. The ethernet throuput was observed to be very low between the clients and the server. This was causing some kind of bottle necking during transfer/fetching of graphics data from the aspect server to the client nodes, for the purpose of building the graphic screens on the operator workplaces. The workplaces on the server would open quickly, whereas the workplaces (Operator) in the clients would mostly open after a very long time or simply hang.
Solution used: Avoid any sort of Link aggregation technique (Bridging,Teaming etc.) and implement RNRP addressing properly in all nodes.
Regards
Rahil
Add new comment