dropping new location structure aspect fails with hint for signal configuration
Hi,
I tried to move a location aspect via drag and drop but it fails with error.
I did following actions.
1) create a new location structure aspect
see pic 1
2) After creating the location structure aspect it is shown in the root node, that's o.k. so far.
see pic2
3) Drag and drop the new location aspect in the node Alarmmanagement
see pic 3
4) A failure message is shown and the action will be canceled
x
5) The following window shows a short description of a failure cause.
maybe somebody has an idea for the problem or a solution.
Thanks!
Answers
This question has not yet been answered.
Add new comment