CBM SCM(CM) Parameter Connection Detection internal coding into CBM editor
Voted best answer
Hello,
Please exaplain in breif for better understanding.
Are you using control diagram with SCM OR direct SCM?
If you want to check the paramter has been used or not in the applications for that you can use search & navigation tool this you can enable it through tools-setup-maintanance-search & navigation here you select the option you need.
if you want to check the parameter connection status for parameter with datatype control connection, you use parameter.controlconnection.forward.connected or status.
Answers
Hi,
It is question when you are programming inputs/outputs into SCM/CM/FB in CBM editor do we have chance to check does parameter is connected when instance has been used... following I'd like to change internal code if port/parameter is not connected without CC data type used...
Add new comment