RTU560 digital tags show date as 7.6.2036 and do not update at SCADA Server
the digital tags defined uner rtu560 show date of 7.6.2036 and the time is also different from that of the Server to which it reports to. whereas the analog tags do work properly. the configuration under replication tab is periodic/ exception.
because of this anomaly in time stamp, the tags do not replicate to the MCS server and further processing.
Answers
This question has not yet been answered.
Add new comment