Aspect Cum Connectivity server installation issue
In SV 6.0.3 of we have (ASCS1, ASCS2 HS & OS1) system in Domain network .
while installation of History service (Data Collector) in ASCS1 it's showing some error but before that, i installed all the system. but now I want to know 1 thing can I format the ASCS1 without affecting my commissioning activity.
Answers
Hi,
If the ASCS2 is running fine with all services, you can troubleshoot the ASCS1. Instead of format, try to troubleshoot the error.
Can you check few things in your 6.0.3 Media?
USB Media\Applications\History\History\RealTime_DB\Project CPIMS\Application\Setup
USB Media\Applications\History\History\RealTime_DB\Base For RTDB Project\Application\Setup
and in both folder check for
App_Install_RTDB_Project.bat
and check for ISO_Date is having current year like 2999
Add new comment