Freelance license and HW-key not working
Installed Combi-station, running in DEMO-mode. Recieved HW-key and licenses.
I have put HW-key in place, and installed licenses for both ES and OS from settings, which was successfully acoording to pop-up.
But, license handling is not working. According to Operations the "hardware key not found". According to license information under help -> about it says "No license installed". (?)
Tried uninstalling and installing again several times, with PC restart in between, then started in both DEMO and production mode. Engineering wont start due to "You dont have a license for this tool". Operations starts in DEMO likewise.
Suggestions would be highly appreciated?!
//Magnus
Voted best answer
Hello Magnus,
take a look in Freelance installation directory Freelance\exe an open the f2k.key file with editor. There is your license installed. compare the license No with the nomber on the hardkey.
Try to copy the license file into the Freelance\exe directory and start the programm.
Combi station is only one license with one hardkey.
If you have two licenses to install, you have two hardkeys to plug in. and two license key nombers in f2k.key.
Which windows version is it?
Bernd
Add new comment