PCA Definition File
Dear supporter,
I have already found the question under following link:
http://72.52.243.203/In-800xA-I-load-...
Is there an answer by now how a PCA Definition File must be created in order to be able to detect and import it using 800xA? I have created a file using the format from the examples in the linked threat, but using the 800xA workspace I am not even able to open it (as it possibly does not detect the PCA format?).
This would be a massive time safer for importing OPC DA object.
Thanks
Answers
Did you load from the Control Connection aspect on the object type?
I believe the load button only light up there.
File support case if you need formal answer.
Add new comment