ACS355 Torque Reference Control
Hi, please could someone tell me what are my options for an external torque control reference. Ideally I would like to set two DI for increasing and decreasing the torque reference. Is this possible, if so how?
Many Thanks
SteveD
Answers
Hi,
Below link of manual for your reference(Page 116).
https://library.e.abb.com/public/1563267283574059bd87947c8b1368aa/EN_ACS355_UM_
D.pdf
Hi Stephen
AFAIK you can obtain one very simple control of torque with the appropriate macro, as the previous one answer.
IMHO the ACS355 is not the better drive to obtain one good torque control.
In any case, with ACS355, you can not use two digital input to increase and decrease the torque, for this performance, the drive has an analog input.
Hope this help you
Add new comment