Advant Controller Node Filtering
We have made some changes to the Node filtering of Alarms on the Connectivity Server RTA Board.
However we are unable to re-boot the AC450 controllers affected.
Does anyone have the procedure to activate node filtering on an Advant controller without having to re-boot it ?
Voted best answer
You have to adjust the master view tables in the controllers with OMVT command. Only reststriction is that you can not use it on MP200 and MP200/1, but you have an AC450.
Add new comment