Unplaced Objects in 800xA
In my FULL BACKUP I get a warning that "Unplaced Objects exist". A afw File is provided there I can see these objects. They don't exist in the system.
A few days before I've created a lot of Log Configurations by Bulk Data Manager. I have done this for 4 similar stations. But, they are not similar, and so by mistake I create Log Configurations for objects that not exist. These are now the unplaced objects.
How I can get rid of these objects?
I have imported them to Lost&Found (with some errors) and deleted them afterwards with no effect. Should I try to delete them by Bulk Data Manager?
Voted best answer
Unplaced object is inconsistent. They are invisible and in practise non-existing within the system, but still the backup tool complains about them. It is known issue. If the object is unplaced, it cannot be located by name using the Find tool, even if its Name aspect still exists (because the name server works with names + structures). Find the object using the GUID in Find tool and delete, either by Delete in the context menu or by pressing the Delete key. Even with Unplaced Object systembackup will not harm anything while restoring.
Add new comment