Ghost node MB300
Dear all,
A custumer has a 800xA 6.0 for Advant controller with AC410, MP200,AC450. In the same MB300 network has AS500, MG230.
In the Dens command show some gosth nodes with subntyp MB100, MB200 and unknow.
What is that? If I delet MB300 gosht nodes are enough to resolv the problem?
Answers
MB100 and MB200 are VERY VERY old communications networks. They have been obsolete for perhaps 20 years. How old is your system ?
MB100 was used before AF100 to communicate to MP51 nodes. In your case that would be Net/Node 4/4
MB200 was Masterbus 200, a predecessor to MB300 for Peer-Peer comms usually between MP200 and Masterview.
Add new comment