MOD300 Enterprise Historian 3.2/1 - Error Message
Hi everyone. We are receiving a error message related to logs collection failure (please see attached image) in our History Server (EH 3.2/1 over Windows 2000).
How to determine which logs are in failure? We have more than 5900 logs
Why is this happening?
I would really appreciate yor comments and help.
Thanks in advance.
Voted best answer
Follow the procedure below to generate a log report and that should have the information of the failed logs,
Running Entry Tables Report from the Command Prompt
This generates a report for all logs and directs the report output to a specified text
file. To run the report, from the DOS command prompt, enter:
c: > hsDBMaint -report > \tmp\filename.txt
where filename is the name of the file where the report output will be directed to.
The file is given a .txt extension. You can view the file using an editor such as
notepad.
Add new comment