PLC Connect Object Trend Value,Min,Max
Implementing a PLC Object Type Library for a customer, I'm not able to have the Object Trend properly getting Value, Range Min and Max. I tried several combinations without success (Property Translation)
The Object Trend aspect should be on the Object level so that I get the Object description.
VALUE is to be retrieved from ./VALUE:Real PCA:Value
MIN is to be retrieved from ./MIN:Real PCA:Value
MAX is to be retrieved from ./MAX:Real PCA:Value
Answers
This question has not yet been answered.
Add new comment