Multiple Faceplates
Hi All,
How can i disable a function where the operator can reopen the same faceplate(same tagname) multiple times?
Requirement:
The faceplate of a specific tag can only be opened once and reopening it from the object or from the aspect link (Control) will only highlight the opened faceplate.
Jelo
Answers
Hi,
Kindly check the "Max number of Windows on screen" in View class configuration of faceplate in library structure.
Add new comment