AC800M AF100 Master setup for communication with APC, DSP not active status
Hi to all experts,
Please advice how to configure CI869 AF100 card as a Master in order to communicate with 6 APC controllers.
We have AC800M+CI869 connected via TC513 to APC. Electrical connection seems to be fine since there is no red error at DSP Send and DSP Receive under CI869 card.
The issue is there is no data exchange.
All DSPs are showing extended status: "Config running, DSP not active".
APC node number match DSP Receive Group.
Idents in APC at AFREC/AFTRA pc elements match DSP positions.
The same DSP configuration was working if AC450 was connected at AF100 as Master.
It seems like CI869 refuses to work as Master.
Current configuration of CI869: Bus 1, Station 80, Time Sync NO, Cable Single, Double DSP Timeout False.
Control Builder version is 6.0.100.27
CI869AF100HwLib 2.11-1
Thank you in advance
Add new comment