MBTCPRead Error Code -6829 Sometimes
I am getting an Error Code -6829 in the MBTCPRead Block Sometimes.
Totally i have used 6 MBTCPRead Blocks.
This error comes in an interval of approx 30 min.
First this error comes in First MBTCPReadBlock and then to other and so on.
I am able to read the values, but some times it is noticed that there is loss in communcation (Once in a day ).
Configuration details:
Modbus TCP is used.
Diagostic Poll time is disabled by setting it to '0'.
Time out is set at "1000ms".
Number of Resend is "3".
Diagonistic Poll Function is "Loopback".
In the Logic MBTCPRead Block Req Pulse : 1s Pulse at a period of 9s.
As per the Error Code in the CBM help File -6829 means "Generic Client timeout aborted"
Why this Error is coming in the MBTCPRead Block ?
Answers
have You tried to use MBTCPReadCyc? Maybe this method will work for You.
How do You have linked all communication blocks in logic?
Add new comment