AC800M controllers sil Level
Hello,
What is the SIL level of ABB AC800M controllers?
Answers
The AC 800M HI controllers can execute code for NonSIL, SIL2, and SIL3. It is the SIL level of the downloaded application that specifies the level.
PM865 + SM810 => capable of executing max SIL2 application (task)
PM865 + SM811 => capable of executing max SIL3 application (task)
by inammel Rank: 57 on 3/5/2018 10:41:23 PM | Like (0) | Report
Edited by Admin:
Add new comment