Migrate Aspect Error SV 800xA5.1
Hi,
I have tried to Migrate Aspect VB to PG2 (using rmc library & AC450 Ctl) at the time showing below the error.
“Failed to migrate contained element “rspDOIndTracking’ (MB300 DO:rspDOIndTracking) because generic elements must be placed on a tool box item in the graphics structure, please see the manual on Subelement and property element migration for more information.”
I tried graphics deploy and migrate but it's not converted PG2.
If can help with above then it would be help or guide me on how to resolve this error?
and i have attached the word documents.
Voted best answer
Kindly follow the bellow mentioned Steps for AC450 Sub elements
Creating Mapping Information for manually created PG generic elements
Mapping information for Generic Element, sub elements, and property
elements are different for PG elements because PG generic element, and VBPG
sub element and property element are not on the same object. To create or
change the mapping information for a PG generic element, perform the
following steps.
1. Start the Graphics Migration Tool.
2. Select the Graphics Structure and locate the PG Generic element. If this
element is not visible, select Show Unmapped Process Graphics in the
Migration Tool. If the element is inherited, go to the object type and execute the
step 3 to step 5 on the generic element.
3. Select Edit Mapping to open the mapping editor.
4. Click Map VB Process Graphic to map a VBPG sub element and property
element to this PG generic element.
5. Update the mapping information and mapping expressions if appropriate.
Answers
Hello,
I suppose rmc library is a product developed by someone else, and that they probably already have a version ready for PG2.
Take contact with the rmc library product owner, for upgrade.
/Ronny
Add new comment