Backup PLC AC500 Program
Hello .. Good evening! I have a PLC ABB AC500 (CPU PM573), software developed in Automation Builder 1.1. And it is in RUN mode and it is not with the memory card plugged in. Can I back up the PLC program by inserting a newly formatted SD card? In case, would the PLC have to create the file structure of the SD card?
Answers
Hi
if you not have the original software you can made only one not editable copy of the application with your SD card
At the follow link one similar question
http://www402.abbext.com/How-download...
For the properties of SD card you can read the attached file
Hope this help you
Is there a software to make a file structure in the newer SD card?
If yes, can you send the link?
i don't have the ABB SD Card.
Source: Software
Hi
ABB SDCARD.ini structure file - for SD card as per the attached file.
This is one simple Text file, editable with Notepad or similar tool.
Hope this help you
Add new comment