800xA Application Server Node
Hi,
What is 800xA Application Server ? Is it allowed to configure application server in redundant configuration mode similar to aspect or conectivity server.
I want to to run one OPC UA server in primary and redundant application server.
In 800xA system level I will configure 2 service providers for each node....does this configuration will help me to achieve the redundancy link.
Any document related to 800xA Application server how to configure ?
Please reply if you have some idea.
Answers
Hello,
when reading 800xA Post Installation manual, you see that Application Server is installed as Conectivity Server and also Redundant Connectivity Server.
I think you will understand by reading that document.
/Ronny
In 800xA application server terminology used for servers like Information Management Server, Batch Server, Asset Optimization Server etc. These server will be added to 800xA system as Connectivity Server.
Hello ,
My understanding is from your question is to run OPC Servers in redundant way. OPC servers cannot be considered as Application servers. OPC servers are meant as Connectovity servers in our 800xA system.
Application server means the servers which are used to do some additional task for the applications in the system such as asset optimization using Asset Optimization servers,Batch applications can run using some Batch Procedure from Batch Servers and some informations to be saved from applications over a long period using Information Management servers.
Add new comment