RNRP 800xA
Hi,
I could able to ping two macines..both are connected to the same physical switch..
IP address 172.16.8.11 and 172.16.8.12.....
when checking the machines in RNRP monitor....machines are not updating in the reachable nodes....
Any idea what could be the reason....
I tried restarting machine.....always it is same......
I am using work group....tried to update the IP's in host file of each mache.....still same result....
Any idea? How it fix ?
Answers
1. Firewall config not made from DVD wizard
2. Factory default Cisco or Westermo switch -> IGMP enabled -> no RNRP -> no xA 5.1+
Hello which version of RNRP is running in the system
ensure RNRP service is running in the local windows service.
Am able to find one bulletin pls follow the same for proper operation of RNRP
3BSE066739_-_en_System_800xA_-_RNRP_Network_Configuration_Requirements
Add new comment