How to configure between 2 network Areas in RNRP using Explicit address
I have a system with 172.16.16.121 and another system with 172.16.128.2
I need the node visibility in RNRP of 172.16.16.121 how to configure vide explicit address 0
Answers
Hi,
use this application, you can solve the configuration issues
by ATP
What is your Subnet ?
by aravind12a6 Rank: 154 on 2/26/2018 11:17:50 PM | Like (0) | Report
255.255.252.0
by ATP
can u clarify that, u need to configure the explicit for 172.16.128.2 ?
by aravind12a6 Rank: 154 on 2/27/2018 12:33:01 AM | Like (0) | Report
I mean I need to view 172.16.128.2 node details in 172.16.16.121 node RNRP
by ATP
Set 1 in no of explicit tab in Base parameter.configure IP, Subnet, Network area. etc. Put the Node number as 258. Try this .
by aravind12a6 Rank: 154 on 2/27/2018 1:50:25 AM | Like (0) | Report
Tried it not working, why 258?
by ATP
Restart the RNrp it should work
by ATP
Put the Node number as 2 , try
by ATP
is ur problem solved
by aravind12a6 Rank: 154 on 2/28/2018 4:29:58 AM | Like (0) | Report
No
by ATP
can u send the RNRP screenshot which is 172.16.128.2 machine
Add new comment