800xA Engineering Workplace
800xA 6.0 Base system license includes one Engineering Workplace which usually is installed on Aspect Server in order to do engineering tasks for the systems - ControlBuilder, GraphicBuilder and so on.
In case of additional laptop is required (like as so called mobie engineering station), is it possible both the server and the laptop to be configured during installation of the system for engineering workplaces with this license?
Is it necessary to order additional engineering workplace license in this case - for example ControlBuilder will be open only in the laptop?
Voted best answer
Hi,
There is no restriction for installation, but product feature will be work as per the license . If you have Graphics builder/ENG_CBM licensed for 2, only 2 users can use Graphics builder/CBM same time. If tried with more users, then license error will be logged.
Answers
Hi,
There is no restriction for installation, but product feature will be work as per the license . If you have Graphics builder/ENG_CBM licensed for 2, only 2 users can use Graphics builder/CBM same time. If tried with more users, then license error message will generate.
Add new comment