ADJUST CLOCK TIME IN PROCESS PANEL 220
Dear Flavio,
Can you help with the Process Panel 220 issue. I found the clock timings not correct and want to adjust in Process Panel 220 diplay. Thanks.
Answers
From MA00571C manual:
"The real-time clock in the operator terminal is set under Setup, Date/Time.
Select the alternative Set Terminal clock. The date and time are now shown. Press
[SET] to change the settings. Enter the desired date and time. In editing mode you
move the cursor with the arrow keys. Press [NEXT] to return or cancel the setting
before pressing [ENTER].
The real-time clock can also be set in run mode through a maneuverable clock object
and during the transfer of projects from a PC to the operator terminal, see the chapter"
Look in the following post how to switch between Program/Run mode, if you don't have an programming software - the clock setting should be there as well:
http://www402.abbext.com/ABB-Process-Panel-220-Keypad-Locked-q13445952.aspx
Source: MA00571C
Add new comment