pid output according to each parameter
hello ,
i have aproject that i want to control the temperature by using afreelance ( AC700f ) controller so i used function block that it called continuous controller ( C_CU )
i make the PID function and simulate it on emulator ( i checked the manual to auto switching , tracking , changing the setpoint and then the output is changed according to CE after this i change the PV and so on ....)
but i can't sure from my setting for each parameter of ( parameter mask 2/3 ) and i need the PID output graph versus each parameter to understand parameter's function and its effect on the output
thank you & best regards
Bishoy Naguib
Control Engineer
MATEC company
Cairo,Egypt
autoeng.bishoy@gmail.com
i have aproject that i want to control the temperature by using afreelance ( AC700f ) controller so i used function block that it called continuous controller ( C_CU )
i make the PID function and simulate it on emulator ( i checked the manual to auto switching , tracking , changing the setpoint and then the output is changed according to CE after this i change the PV and so on ....)
but i can't sure from my setting for each parameter of ( parameter mask 2/3 ) and i need the PID output graph versus each parameter to understand parameter's function and its effect on the output
thank you & best regards
Bishoy Naguib
Control Engineer
MATEC company
Cairo,Egypt
autoeng.bishoy@gmail.com
Voted best answer
Answers
I agree with Sumit the best way to expose any property is creating a User Function Block. Use the example indicated in the previous answer.
I would strongly recomend consulting the documentation - it explains all parameters used in functions and blocks quite clearly. I took the liberty to attach info which should be helpful to You.
Source: 3BDD012514R0501_Functions and FBs
Add new comment