Is possible to mix virtual and real servers in 800xA?
In already working 800xa system I need to replace a part of servers due hardware fail. Now is very esy to use virtual servers but I cant repalce all server yet. Can work togheter real and virtual servers where a primary server is real and their redundant is a virtual server?
Answers
Hi,
It is possible, doesnot mater about the Physical or Virtaul. It should be in same Domain and the network configuration should be recommended as per 800XA.
Yes it is possible to mix several servers in a 800xA, we have some systems where the connectivity servers are running virtualized. You need to take care of every requirment that are indicated on manual 3BSE056141-510_en_System_800xA_5.1_Server_Node_Virtualization.
Add new comment