Freelance 2016
Hej jag har precis installerat Frelance 2016 på en Vm med windows 7.
när jag vill öppna enginaring tool får jag frågan om User och Password.
Kan inte minnas att jag skrev i något sådant vid innstallationen.
vart får jag reda på det eller behöver jag göra om innstallationen
vid installationen valde jag
enginaring & operativ med alla tillläg
/Robert
Hi, I have just installed Frelance 2016 on a Vm with Windows 7.
When I want to open the ingenaring tool, I get the question about User and Password.
Can not remember that I wrote something like this at the installation.
where do I get it or do I need to reinstall the installation
At the time of installation, I chose
ingenaring & operative with all additions
/ Robert
Answers
Hej,
har du kollat General Settings, auto login ?
/Ronny
I think you have installed all options of the CBF installation.
So you also installed the security lock.
With security lock you have to give permission for configure.
Or change the installation without security lock.
Add new comment