800xa CEt crash on opening management
HI. In a 800xA 6.0.1 installation i've import an scd file. When i try to open the management interface i get the following error (see the attached screenshot) :
'Computer Node: Unable to cast COM object of type 'System.__ComObject' to interface type 'Interop.GwManagement.IGwConfiguration'. This operation failed because the QueryInterface call on the COM component for the interface with IID '{F5691AA4-0722-4E95-BE92-C7721ECB4CE6}' failed due to the following error: No such interface supported (Exception from HRESULT: 0x80004002 (E_NOINTERFACE)).'
Best Regards
Answers
Hello,
the CET software needs to be uninstalled and reinstalled.
/Ronny
This is an issue with CEt software installation along with the SQL server.
The interface bwtween SQL server and CET tool has broken it seems.
So we need to uninstall the CET software along with SQL server and reinstall both.
Regards
Manoj
Add new comment