How to add CM592-DP in "Device repository"
I use PS501 Control Builder Plus 2.3.0 Release Build 339 (Part of Automation Builder 1.0.4).
In my project I use a PM573-ETH and want to add the CM592-DP communication module.
How will I do to add this module in "Device repository"?
I upgrade Automation Builder from 1.0.1 to 1.0.4 but that not solve the problem.
Answers
Hi
AFAIK you can use the new module CM592-DP only with Automation Builder 2 and later.
IMHO with old version of AB such 1.0.4 you need to use the old type CM572-DP module
Hope this help you
Add new comment