How can I load a project in a station of digivis operations without Graphics Builder?
Hello,
I have an station with the digivis operations, but I don't have the graphics builder in this PC.
I try to copy the file .pro in the proj directory of the station, but this don't works.
Anybody knows other way to update the project without the graphics builder?
Thanks in advance.
Voted best answer
Hello,
If I understood correctly, You have DigiVis operator station but no Control Builder F in that PC ?
In such case you can’t add your graphic to operator station, just by copying .pro file.
You can add graphic in digivis operator station from Eng. station i.e from CBF. Follow this procedures go to CBF > Project Tree > DigiVis resource (VIS) > you can add new graphic from Rclick (FGR) or you can add Common Display Pool(PCD) and FGR under that. Either design your graphic or import it and after linking your variables make plausibility check through then go to running mode and make change load object to your VIS resource. Your added graphic will be displayed on DigiVis operator station. If you have manuals I suggest pls go through procedures and configuration for Operator station.
Hope it helps to you……..
Answers
in Freelance system we do not use a name graphic builder...
Engineering station called Control Builder F or CBF for short is used for anything and everything including graphics.
Every single Freelance system delivered World-wide has been sold with CBF license - it should be somewhere in your plant (or depending on the contract, the System Integrator who delivered the project might have it)
If you wish to have a quick check/test/education etc, you may use the free of cost demo version of the software that is fully functional for 100 days, after which you may reinstall the software and use it for educational purposes.
Request Freelance Quickstart (including freelance software) from your local ABB office or your nearest ABB Authorized Value Provider
Add new comment