CBF and DigiVis (Freelance 9.1) on the 64 bit system
I have a computer 64 bit with Windows 7 on it. Also I have a Freelance 9.1 software (only 9.1 without any upgrade).
What should I do?
Downgrade Windows 7 (64 bit) to Windows XP (64 bit) and install Freelance software on it
OR
downgrade Windows 7 (64 bit) to Windows XP (32 bit) and install Freelance software on it.
Thank you for your answers.
Answers
Hi
Reference to the image below, you can use Freelance version 9.2 sp2 for window 7 64bit
Hi,
The Release Notes of Version 9.1 states the following:
Freelance 800F Version 9.1 has been released for use with the operating system
Windows XP Professional SP2
During the test phase Microsoft has released Windows XP ServicePack 3. This
version could not be taken into account for this release. The compatibility of
Freelance 9.1 with Windows XP Professional SP3 will be tested after the release
and the results will be distributed.
Starting Freelance 9.1 + Roll Up 1a the Support of Windows XP Professional SP3 is included, however I believe that the 64 Bit support was not included. It is usually necessary even to have the PC HW itself supporting 64 Bit just to use the respective Windows XP version on it.
I think the that the Roll Up does not need an extra license.
Add new comment