I am trying to install control builder m professional 5.1 available with 800xa its giving error, install 800xa
Answers
Greetings,
Could you please give more information about the error, like screentshots etc. ?
I sure hope you are following some kind of installation user's guide?
CBM included with System 800xA does NOT work without main System 800xA software and a running system/server. Software from the System 800xA suite is most easily installed with the included automated system installer which takes care of everything for you incl 3rd party requirements (which I guess you have problems with).
Compact Control Builder on the contrary do work outside the realm of System 800xA and has a more or less "one button installer".
/Stefan
Hello,
Try to adhere to manual for installation.
There are certain prerequisites to be taken care thn only it will result in successful installation of CBM.
Try to go into error details and thus it will show you missing requisites.
Regards
If you need to install just Control Builder (not all 800XA) you need to install compact control builder option.
Insert your 800xA installation DVD you can check if your windows is ready by the system checker tool provided.
Install the 3rd party software needed like mssql, visual basic... Provided in the 3rd party software in 800xA DVD
Before to install the control builder and other 800xA software components in the dvd.
Add new comment