800xA 5.0 Advant Trend on Grpahic Mimic
We have 800xA 5.0 System with Advant Connect ,
Presently the customer using Graphic primitive Advant Trend Trim for Showing trends of specified timing on Grpahic mimic,
But when the grpahic page is refreshed and he comes back to the same page the trend data starts from that point of time (note: log configurations are avialable for the selected variable)
Is there any property needs to be changed or Any other Element available to keep the trend running in the background like the one's in 5.1 PG2.
Answers
In VB graphics, you can embed the Object Trend display into the Operator Display using an Aspect View Ctl (iirc its on the "Special Elements" tab of the graphics builder toolbox)
Theres a performance cost. You're basically opening 2 graphics.
Add new comment