How to use Digital I/Os on SM811?
How do we use the digital I/Os that are configured on the SM811 in our ESD logic?
Like i wish to use the Access Enable and Reset All Force DIs on the SM811 in my logic, which paramter can i access for these parameters?
Voted best answer
Access Enable and Reset All Forces are available as variables "AccessEnable" and "SMResetControllerForces" in both ForcedSignals function block and ForcedSignalsM control module. Simply add the function block or control module in your program.
Add new comment