How I can achieve redundency AC500 PLC PM573-eth to AC500 PLC PM573-eth ..??
Answers
Dear Peter,
the AC500 redudancy can be achieved by using a cable, High Availability library. Using the CS31 bus. Thats it.
For more Information pls refer www.abb.com
Or give me a call
Rgs. Wangelis
If you are talking about hot redundancy, Abb suggests one use PM58x and above cpus.To achieve controller redundancy, a high availability module such as ci590 cs31 ha is required to interface the controllers in a redundant configuration.in addition to the above hardware, HA library functional blocks namely, cs31_HA CONTROL, DATA_SYNC and callback_stop are essential.
Rahil Mohammed
Add new comment