Importing whole array tag in CP600-eco
Hello
i need to import the whole array into CP600 eco panel builder. I couldnt import as whole array instead i am able to import as individual array element. i need to display values in scatter diagram and it supports only whole array tag as x and y elements. i use codesys-eth protocol and import tags using symbol file exported from automation builder. Any help is appreciated. i use latest software version and CP607 HMI.
Answers
Hi,
I use Modbus TCP protocoll, but imagine it is the same way to do it.
This is how I do it:
1. I take a Export from an example tag in .xml format.
2. Use MS Excel to Open the .xml file and insert all the new tags.
3. Save the document as XML Data(*.xml)
4. Import in panelbuilder
Add new comment