One CI867 as Master and Slave
I have a requirement in wherein two 3rd party package interfaces are connected to the same AC800M with a single CI867. One of the interface has ABB system as the master and the other needs ABB system as slave. Is it possible to have the same CI867 act as master for one package and slave for another?
Voted best answer
Greetings,
Yes, it is possible to use both master and slave at sametime for CI867.
There is a parameter called "Modbus Slave Enable", if it is set to True. CI867 Card acts both master for one package and slave for another package.
For more details please see below picture:
Hope it helps you.
by admin Rank: 44 on 5/11/2015 8:06:02 PM | Like (0) | Report
If you got an answer then pls vote for an answer and help in closing this thread.
-Admin
Add new comment