[Error] Operation rejected by "ObjectName":Library Member (Object hook: Change)
When I do some changes on an specific CMT, I get the following Error message and I can't save the modification:
[Error] Operation rejected by "ObjectName":Library Member (Object hook: Change)
The Next message is:
"The source code operation has encountered an error"
Answers
Usually this is because you are trying to use the object in a way that is not allowed.
The object hook aspect is used in composite objects to control how the module type gets instantiated into the variaous structures like the control and functional structure.
Usually there isnt a specific solution for this problem. You just have to figure out which operation is not allowed and find another way to do what you want to do.
This is a very generic issue that comes due to wrong workflow. Could you attach a screenshot or log file?
by backdraft
this can be nearly everything, to get help about the specific problem you face please add Information about what Aspect or Object you are changing, what Aspects are existing on the Type and some Screenshots if possible as well
Add new comment