400 Connectivity Server
Hi All,
I have a synchronization problem with the plant explorer in the 400 Connectivity server.
The problem is RTA Board aspect in the 400 Connectivity server is working fine, showing all the controllers status and able to see the data.
But when I open the same RTA board aspect in other servers like aspect or IM or any other server other than 400 Connectivity server, It is showing status of RTA board as timeout and not showing any controllers status. Aspect is totally blank.
I have restarted all the servers, but no luck.
Could anyone help me resolving the above issue.
Thanks in advance
Voted best answer
I believe its time to engage your regional ABB support center.
Have the restored server gotten another IP address? Is the hosts file or DNS having wrong information?
What OPC quality do you get in Process Graphics diagnostic window (use Shift to show the Diagnostics menu item if using an operator workplace).
Answers
Has 800xA for Advant Master Connect been newly added to this system? Have you forgot to install it in the clients?
Is affinity configured? Have you forgot to include the 400 CS in the list of servers?
To avoid accidentally locking out a server, always keep the "All nodes" group last on each affinity row.
I have deleted the RTA board from the control structure.
And when i try to create new one, it is showing one error like below:
Failed to create the object.
E_AFW_AOM_Object_not_found(0x8abb090a) object not found in the object manager.
Could anyone help me in resolving the issue.
Thanks in advance.
by Sridhar C Rank: 82 on 3/9/2015 12:18:51 AM | Like (0) | Report
I have deleted the RTA board from the control structure.
And when i try to create new one, it is showing one error like below:
Failed to create the object.
E_AFW_AOM_Object_not_found(0x8abb090a) object not found in the object manager.
Could anyone help me in resolving the issue.
Thanks in advance.
Add new comment