AC500 and CM574-RS both in master mode (modbus)
Goood day, everyone!
Is sabj real? Can we configure AC500 (PM573) and CM574-RS ports as master for modbus protocol?
And another question, can we configure two ports on CM574-RS as master for modbus protocol?
Thanks for your answers.
Is sabj real? Can we configure AC500 (PM573) and CM574-RS ports as master for modbus protocol?
And another question, can we configure two ports on CM574-RS as master for modbus protocol?
Thanks for your answers.
Voted best answer
Yes, all COM ports on PM573 and CM574 can be configured as Modbus Master, independently.
Modbus Master is called Client in COM Modbus settings in HW configuration.
In the application you will need different COM_MOD_MAST blocks
Add new comment