Safeguard alarm-event Configuration
Hi,
We have installation of safeguard system with xa 4.1 system.
I am getiing question mark "?" at condition column of alarm list of analog inputs only.
I have checked Event 1 to 20 and other configurations. only Signal error (in S3) is configured in events.
I should be getting LIM1 or LIM 2 message or any user defined message in condition column.
where i can configure LIM1 or LIM 2 configurations in Event configuration. is there any refernce manual to configure events in safeguard. (Details of s1, s2 and s3 of event configuration element)
Thanks
Voted best answer
Hi Dash
The manuals might help you:
1) 800xA for Safeguard 5.0 SP2 Configuration
2) 800xA for Safeguard 5.1 Configuration
3) 800xA for Safeguard 6.0 Configuration
BR Carsten
Add new comment