AC400 Series OCS Screens
Hi,
we want to replace an Advant OCS application (AC450 + OCS) with 800xA using '800xA for Advant Master'. In document "3BSE030340R5021_en_System_800xA_5.0_SP2_Advant_Master_Configuration.pdf" there is a description on how to use the 'Display Converter' VB6 addin for convering the advant screens. But what files (where they are located) and how can i get them from the Advant OCS (Unix workastation) ?
Answers
The advant display are held in the .ds and .g files in the displays directory of your advant stations.
There are several ways to get them from the advant station to the PC, but the most common way is to transfer them over an ethernet connection using "Kermit" http://en.wikipedia.org/wiki/Kermit_(protocol) or "ftp" http://en.wikipedia.org/wiki/Ftp which are file transfer protocols supported by both Unix and Windows.
Add new comment