Im having ci867 with ac800m, in that ch2 is connected to HMI (which is Modbus slave),can i use ch1 as Modbus slave
In CI 867 ch2 is having a modbus slave connected to it(cp400 HMI), I have changed the ch1 IP to different subnet and tried establising a connection with pesudo master (actual purpose is to get read the data from quantum plc with NOE using i/o scanning)softwares,(i can ping that ip ). but im not getting any data out of it?Is there any other configuration to be done on abb plc to be act as modbus tcp server. Kindly help?
Answers
is there one app that could be help
Add new comment