ABB Freelance emulator doesn't work
For a school project we need to work with ABB freelance.
But the Freelance Controller Emulator Service won't start on my laptop.
When I try to start the emulator manually I get this error
Translated:
Freelance Controller Emulator Service can't start on the local computer.
For more information check the system log.
If the service is not published by microsoft, contact the publisher of the service.
Mention the service specific errorcode 9.
I hope someone can help me fix this.
Kind regards,
PA Group C
Answers
Hi,
There are 3 different ways to open/run Freelance emulator, before that please check the emulator service is started or not, if not please start the same.
1.Open IE, type http://localhost:8888/
2.Open IE, type http://127.0.0.1:8888/
3.Open IE, type http://pc ip address:8888/, for eg: http://172.16.x.x:8888/
Add new comment